Technical FAQs

Ask a Question

Does Schneider Electric offer NEMA Type 1 Heavy Duty Safety Switches without knockouts?

Issue:
Does Schneider Electric offer NEMA Type 1 Heavy Duty Safety Switches without knockouts?

Product Line:

Heavy Duty Safety Switches

Environment:

Understanding the product features

Cause:
Need for field cut openings for conduit entry

Resolution:
All NEMA Type 1 Heavy Duty Safety Switches, 30A - 200A are provided with knockouts. All NEMA Type 1 Heavy Duty Safety Switches, 400A - 1200A are provided with no knockouts. For 30A - 200A indoor applications requiring no knockouts, a NEMA Type 12 safety switch could be used in the NEMA 1 application. The NEMA Type 12 (suffix AWK) safety switches are not provided with knockouts. Do not confuse with NEMA Type 12K (suffix A) safety switches, which are provided with knockouts.
Was this helpful?
What can we do to improve the information ?