Technical FAQs

Ask a Question

Do we have a power dissipation rating curve for the Altivar Drives?

Issue:
Trying to determine the heat dissipation at varying speeds.

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
Heat dissipation curves for drives.

Resolution:
There is nothing published however it is mostly linear but there is a fixed amount of power to run the controls and fans. So imagine a curve that starts a bit above zero and then goes linearly up to 60 Hz. 

Was this helpful?
What can we do to improve the information ?