Technical FAQs

Ask a Question

What is the difference between a Q2M2200MT and a Q2M2200MB?

Issue:
What is the difference between a Q2M2200MT and a Q2M2200MB?

Product Line:

Circuit Breaker

Environment:

Need to discern between the two similar breakers

Cause:

Assure correct breaker is identified

Resolution:

The MT suffix would indicate that lugs are provided on the ON end of the breaker, with studs on the OFF end of the breaker for connection to busbars below the breaker.
The MB suffix would indicate the lugs are provided on the OFF end of the breaker, with studs on the ON end of the breaker for connection to busbars above the breaker.
Was this helpful?
What can we do to improve the information ?