Technical FAQs

Ask a Question

What are the repair parts for a HOM1632M150TC, Series S03 load center?

Issue:
What are the repair parts for a HOM1632M150TC, Series S03 load center?

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - HOMC20UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K
Door Latch Kit  - 4020284450K
Interior Assembly - 40565-083-51 (Interior assembly does not come with the main breaker, see below main breaker)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2150VH
Equipment Ground Bar - PK18GTA and LK100AN
Was this helpful?
What can we do to improve the information ?