Technical FAQs

Ask a Question

Can the QO2TR be padlocked in the ON or OFF position?

Issue:
Can the QO2TR be padlocked in the ON or OFF position

Product Line:
QO Circuit Breaker Enclosure

Environment:

Can the QO breaker installed in the QO2TR be padlocked

Cause:
Understanding the locking capability of the QO2TR

Resolution:
The QO2TR is an enclosure for a field installed 2P QO circuit breaker. The cover of the enclosure can be padlocked closed, but a padlock attachement cannot be used with the installed circuit breaker. The enclosure is too small for the cover to be installed when a padlock attachment is attached to the enclosed circuit breaker.

Was this helpful?
What can we do to improve the information ?