Technical FAQs

Ask a Question

Where can I find line current max values for the ATV312 drives?

Issue:
Where can I find line current max values for the ATV312 drives?

Product Line:
Altivar ATV312

Environment:
All

Cause:
Input line currents for the ATV312 drives.

Resolution:
See the ATV312 install manual document " bbv46391 " , for line current max values.
The input line supply values are going to be for voltages between 200VAC to 240VAC or  380VAC to 500VAC 50/60hz.
 

Was this helpful?
What can we do to improve the information ?