Technical FAQs

Ask a Question

M-flex system is not running in hand mode.  Drive stays at RDY state when called to run in hand mode.

Issue:
Enclosed drive is not running properly after initial installation.  Drive is not responding to commands.  Control wiring has been verified as correct.

Product Line
E-flex, M-flex, S-flex, IFD field drives and other enclosed Altivar/Altistart products.

Environment:
Initial startup of enlosed drive and/or SoftStart products.

Cause:
Recomendation of actions to be performed at initial startup.

Resolution:
It is recommended at initial startup of enclosed Drive / SoftStart systems that the system be checked for loose wires or terminators that may have loosened during shipping.   The system should be checked thouroughly for loose connections before power is applied to the system for the first time.
Was this helpful?
What can we do to improve the information ?