Technical FAQs

Ask a Question

What are the repair parts for a HOM30M100C, Series S03 load center?

Issue:
What are the repair parts for a HOM30M100C, Series S03 load center?

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - HOMC30U125C
Cover Mounting Screw - 4020513002K (6 required)
Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
Interior Assembly - 40565-479-51 (Interior assembly does not include the main breaker, see below main breaker)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM100VH
Was this helpful?
What can we do to improve the information ?