Technical FAQs

Ask a Question

Are double throw safety switches available in Type 316 stainless steel enclosures?

Issue:
Enclosure for corrosion resistance

Product Line:

Double Throw Safety Switch

Environment:
Type 4X

Cause:

Enclosure needed for the environment at the installation

Resolution:

No, Schneider Electric does not offer Double Throw Safety Switches in Type 316 stainless steel enclosures. We do offer a limited number of Double Throw Safety Switches in Type 304 stainless steel enclosures. Refer to the latest Schneider Electric Digest for selection.
Was this helpful?
What can we do to improve the information ?