Technical FAQs

Ask a Question

How do you set up and route through SY/MAX NIM modules to a SY/MAX PLC using 8010 SFW572 WINMATE Software?

The first 3-digit number represents the source. The source is the connection point between the personal computer

and the Network. The last 3-digit number represents the destination. The destination is the connection point between
the SY/MAX processor and the Network. The first digit of the 3-digit number indicates the port on the NIM
(Network Interface Module) to which the computer or processor is connected. The first digit can be a 1 or 0, indicating
one of two ports on the NIM.

Example

Shown below is a simple routing path from a PC through 2 NIM modules


Legacy KB System (APS) Data: RESL174994 V2.0, Originally authored by DiSa on 05/23/2012, Last Edited by BrWa on 05/23/2012
Related ranges: SY/MATE
Was this helpful?
What can we do to improve the information ?