Technical FAQs

Ask a Question

How much internet bandwidth is my Wiser system using?

Issue:
How much internet bandwidth is my Wiser system using?

Product Line:
Wiser Home Management System
 
Environment:
https://www.wiserenergy.com
 
Cause:
Customer is concerned about the amount of data that the Wiser system may be transmitting. 
 
Resolution:
The Wiser Home Management System uses very little internet data.  Within the home, the devices commincate to the Gateway via Zigbee radio technology.  Thus, no internet communication occurs among the devices within the home.   Internet communication occurs every 15 minutes as the Gateway reports device data up to the Wiser servers.  These communications are less than 50kB, consisting of numerical energy data for last 15 minute time interval. 
Was this helpful?
What can we do to improve the information ?