Technical FAQs

Ask a Question

How can I set my Wiser thermostat for Energy Star guidelines?

Issue:
How can I set my Wiser thermostat for Energy Star guidelines?
 
Product Line:
Wiser Home Management System
 
Environment:
https://www.wiserenergy.com,  EER56000, EER56100, EER58000
 
Cause:
Customer would like to make sure his thermostat is set at or better than Energy Star guidelines.  
 
Resolution:
To optimize between comfort and energy savings, pre-configured Energy Star templates for both heating and cooling are available through the Wiser portal, www.wiserenergy.com.   From the Thermostats tab of the portal, scroll to the bottom and select "Energy-Saving Templates".
Was this helpful?
What can we do to improve the information ?