Technical FAQs

Ask a Question

Do I need internet to use my Wiser thermostat?

Issue:
Customer does not have internet service in the home, but wants to use a Schneider Electric Wiser Thermostat.   Another possible issue is that customer has internet, but does not have a Wiser Gateway Device.
 
Product Line:
Wiser Home Management System
 
Environment:
Wiser Thermostats, EER56000, EER56100, EER58000
 
Cause:
Internet service is not available.
 
Resolution:
Wiser thermostats are intended to have internet access.  However, these thermostats can control an HVAC system as a standalone device with no internet connection.   Without internet connections, features such as scheduling and setpoints must be programmed through the thermostat keypad and LCD screen.     

****   A Wiser Coordinator (EER21200) is required to link the Thermostats (EER56000, EER56100, EER58000) to the internet.  ****
Was this helpful?
What can we do to improve the information ?