Technical FAQs

Ask a Question

I want to start, stop, or change the frequency of Wiser Energy Alert emails.

Wiser System owner wants to change his email preferences.  

Product Line:
Wiser Home Managment System


Wiser Account settings are not correct. 

1.  On the Profile tab of, click Account Info.  Update email preferences for E-News, Product Announcements, Promotions.
2.  On the Energy tab, go to the Goal Section and update preferences for budget alerts.
3.  In order to change the email address, go to the Profile Tab, Account Info.   Select Update Account Information to change the primary email address.   Secondary email addresses can be added, editted, or removed under the Address Book of the Profile Tab.

Was this helpful?
What can we do to improve the information ?