Technical FAQs

Ask a Question

Does Schneider Electric offer a 400A, EZM branch meter with a Bolt-On meter socket?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Branch Meter Sockets 

Cause:
Application

Resolution:
Yes, The 400amp EZM Meter Branch devices are available with a K-Base Bolt-On meter socket, in 1 PH In/1 PH Out, 3PH In/1 PH Out and 3 PH In/3 PH Out, in 1 or 2 meter socket arrangements. The prefix of the catalog numbers is EZMK, refer to the latest Schneider Electric Digest for selection of complete catalog numbers. 


 

Was this helpful?
What can we do to improve the information ?