Technical FAQs

Ask a Question

What is the ampere rating of the circuit breaker for an Enclosed 22 soft start?

Issue:
300 horsepower Enclosed 22 circuit breaker ampere rating.

Product Line:
Enclosed 22

Environment:
ATS22 soft starter 

Cause:
Replacement parts and ratings.

Resolution:
Circuit breakers are listed in the instruction bulletin 30072-453-26 for the Enclosed 22.
Most other components are also listed.
http://www.schneider-electric.us/en/download/document/30072-453-26/

Was this helpful?
What can we do to improve the information ?