Technical FAQs

Ask a Question

What are the repair parts for a HOM4252L200TC, Series S03 load center?

Issue:
What are the repair parts for a HOM4252L200TC, Series S03 load center?

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - HOMC42UC
Cover Mounting Screw - 4020513002K
Door Hinge - 4028356450K
Door Latch Kit 4020284450K
Interior Assembly - 4056591851 (Interior assembly does NOT include the main lugs, see below main lugs kit)
Main Lugs Kit - QOL225
Neutral Bonding Screw - 4028345850K
Ground Bar - (2) PK15GTA and LK100AN
Was this helpful?
What can we do to improve the information ?