Technical FAQs

Ask a Question

What are the repair parts for a HOM1632L200TCFT Series S03 load center?

Issue:
Previous design repair parts

Product Line:
Homeline Load Centers

Environment:
Repair Parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - HOMC30UC
Cover Mountig Screw - 4020513002K
Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
Interior Assembly - 4056549451 (Does not include the Main Lugs, see main lug kit below. BUT it does include the Feed Through Lugs Both Phase and Neutral)
Main Lugs Kit - QOL225
Neutral Bonding Screw - 4028345850K
Equipment Ground Bar - PK23GTA 

NOTE: This Load Center is Obsolete and No Longer Available. Consider the QO12436L200TFT with the cover QOC40UF.
 
 
Was this helpful?
What can we do to improve the information ?