Technical FAQs

Ask a Question

How does the InH fault inhibit assignment work on the ATV61 and ATV71 drives?

Issue:
How does the InH fault inhibit assignment work on the ATV61 and ATV71 drives?

Product Line:
Alitivar ATV61 and ATV71

Environment:
All

Cause:
Needs to have an input that disables all faults for an firemans override.

Resolution:
1.8 Menu Fault inhibition hold the enter button down for 2 seconds to program.
The logic input that s assigned to InH input when turned on will make fault the monitoring inactive.
When the input goes back to 0 or off the fault monitoring is active again.

Caution:
-Inhibiting faults results in the drive not be protected.  This voids warranty on the   drive.
-Check that the possible consequences do not present any risk.
-Failure to follow these instructions can result in equipment damage.

Was this helpful?
What can we do to improve the information ?