Technical FAQs

Ask a Question

What is the catalog number for the protective covers for power terminals on the ATS22 softstarts?

Issue:
What is the catalog number for the protective covers for power terminals on the ATS22 softstarts?

Product Line:
ATS22  Altistart 22

Environment:
All

Cause:
Missing protective covers.

Resolution:
LA9F702 for ATS22C11S6/S6U, ATS22C14S6/S6U, ATS22C17S6/S6U
LA9F703 for ATS22C21S6/S6U, ATS22C25S6/S6U, ATS22C32S6/S6U, ATS22C41S6/S6U, ATS22C48S6/S6U, ATS22C59S6/S6U
Each part number has a set of 6 terminal covers.
 
Was this helpful?
What can we do to improve the information ?