Technical FAQs

Ask a Question

Can you run the Altivar drives with the default programming settings?

Issue:
Can you run the Altivar drives with the default programming settings?

Product Line:
All

Environment:
All

Cause:
No access to the motor nameplate information

Resolution:
No it is not recommended to bypass entering the motor name plate information. The default motor data will not match your motor name plate information.  Its very important to set up and program the motor name plate data into the drives simply start menu 1.1.

If you do not have complete programming manual for your drive you can search online in any search engine the words example: "ATV312 programming manual"


 
Was this helpful?
What can we do to improve the information ?