Technical FAQs

Ask a Question

How much aluminum and zinc by weight and by surface area ?

Issue:
How much aluminum and zinc by weight and by surface area ?

Product Line:
ATV71HU55M3

Environment:
All serial numbers

Cause:
Not published

Resolution:
ATV71HU55M3 weight is 5.5kg.
- alluminium alloys are 12.5% which makes 687.5g
- zinc is not mentioned, means it is not used or amount is up to 33g
(total sum is 99.94% so max. it could be: 0.06% * 5500g).

We do not have information concerning surface.

Was this helpful?
What can we do to improve the information ?