Technical FAQs

Ask a Question

What is the part number and description for Elapsed Time Meter (option B08) on an Enclosed ATS22 unit?

Issue:
What is the part number and description for Elapsed Time Meter (option B08) on an Enclosed ATS22 unit?

Product Line:
ATS22 Altistart

Environment:
All

Cause:
Request for timer reset.

Resolution:
The part number is 2640312030. It is made by Kessler-Ellis, model H57.
It provides a Seven-digit analog, non-resettable elapsed run time meter.
Not available on Type 3R enclosures.
Was this helpful?
What can we do to improve the information ?