Technical FAQs

Ask a Question

Are the MD motor disconnect switches pad lockable?

Issue:
Are the MD motor disconnect switches pad lockable?

Product Line:
Enclosed motor disconnect switches

Environment:
MD Motor Disconnect Switches: MD3304X and MD3604X

Cause:
Product feature, Product requirement
 
Resolution:
Yes. A padlock can fit through the rotary handle when it is in the off position to prevent it from turning.
Was this helpful?
What can we do to improve the information ?