Technical FAQs

Ask a Question

Is there a way for the VW3A1101 remote HMI used with a ATV32, to display motor speed as a percentage, not frequency?

Issue:
Is there a way for the VW3A1101 remote HMI used with a ATV32,  to display motor speed as a percentage, not frequency? 

Product Line:
Altivar 32

Environment:
All models equipped with VW3A1101 remote HMI, All serial numbers

Cause:
Information not included with the quick start guide for the ATV32 series drives.

Resolution:
The VW3A1101 can not be configured to display motor speed as a percentage when connected to the ATV32 series drives.  It can only be displayed in Hertz.

Was this helpful?
What can we do to improve the information ?