Technical FAQs

Ask a Question

Why is "0" the factory setting for F695?

Issue:
F695 is the High Frequency setting for the Analog Output but the factory setting is 0

Product Line:
ATV21 and ATV212

Environment:
All models and serial numbers

Cause:
None

Resolution:
In fact when F695 = 0hz it acts for the scaling using FH (maximum frequency), so if you have set a different value of FH than 50Hz or 60Hz and your motor is running at 50Hz for nominal speed, you have to adjust this parameter for scaling

Was this helpful?
What can we do to improve the information ?