Technical FAQs

Ask a Question

What software programming options are available for the ATV21 drives?

Issue:
What software programming options are available for the ATV21 drives?

Product Line:
Alitvar ATV21

Environment:
All

Cause:
Test and programming software package for the ATV21 drives.

Resolution:
PC soft software works with the ATV21 and ATV212 drives
SoMove software works with the ATV212 not the ATV21.

http://www.downloads.schneider-electric.com/sites/oreo/ww/document-detail.page?p_docId=2331176&p_Conf=i#http://www.downloads.schneider-electric.com

optional cable is part number VW3A8106 or TCSMCNAM3M002P

Was this helpful?
What can we do to improve the information ?