Technical FAQs

Ask a Question

What are the repair parts for a HOM30L150TC, Series S03 load center?

Issue:
What are the repair parts for a HOM30L150TC, Series S03 load center?

Product Line: 
Indoor Homeline Main Lugs Load Centers

Environment: 
Repair parts

Cause: 
Maintenance

Resolution:  
Only the parts listed below are considered field replaceable.
  • Cover - HOMC30UC
  • Cover Mounting Screw - 4020513002K
  • Door Hinge - 4028356450K
  • Door Latch Kit 4020284450K
  • Interior Assembly - 40565-086-51 (Interior does NOT include main lugs, obtain main lugs kit below)
  • Main Lugs Kit - QOL225
  • Neutral Bonding Screw - 4028345850K
Was this helpful?
What can we do to improve the information ?