Technical FAQs

Ask a Question

What are the repair parts for a HOM30L150C, Series S03 load center?

Issue: 
Current design repair parts

Product Line
Indoor Homeline Main Lug Load Centers

Environment:   
Repair parts 

Cause: 
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
  • Cover - HOMC30UC
  • Cover Mounting Screw - 4020513002K
  • Door Hinge - 4028356450K
  • Door Latch Kit 4020284450K
  • Interior Assembly - 40565-086-51 (interior does NOT include main lugs, obtain main lugs kit below)
  • Main Lugs Kit - QOL225
  • Neutral Bonding Screw - 4028345850K
Was this helpful?
What can we do to improve the information ?