Technical FAQs

Ask a Question

What are the repair parts for a HOM12L125C, Series S03 load center?

Issue: 
What are the repair parts for a HOM12L125C, Series S03 load center?

Product Line:  
Indoor HOMELINE Main Lug Load Centers

Environment:  
Maintenance

Cause: 
Load center repairs

Resolution:   
Only the parts listed below are considered field replaceable.

Cover - HOMC12UC
Cover Mounting Screw - 4020513002K
Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Interior Assembly - 40565-073-51 (Interior does NOT include main lugs, obtain main lugs kit below)
Main Lugs Kit - QOL125
Neutral Bonding Screw - 4028345850K
 
Was this helpful?
What can we do to improve the information ?