Technical FAQs

Ask a Question

What is the functional replacement for ATV58 series?

Issue:
What is the functional replacement for ATV58 series?

Product Line:
Altivar 58

Environment:
All

Cause:
Obsolete, no longer available.

Resolution:
For variable torque applications recommendation ATV630 series.
For constant torque applications recommendation ATV930 series
Please note the replacement ATV630 and ATV930 drives may not fit into an existing enclosure like the Econoflex, MCC or 58M enclosures.  If you have an existing enclosed product you will need to replace the complete enclosure or send the old drive into the repair depot for the repair. 
 

Was this helpful?
What can we do to improve the information ?