Technical FAQs

Ask a Question

How do you remove the bottom cover on the LHP ATV61 drives?

Issue:
How do you remove the bottom cover on the LHP ATV61 and ATV71 drives?

Product Line:
Altivar ATV61 and ATV71 LHP

Environment:
All

Cause:
Removing the bottom plate on the LHP ATV61 drives.

Resolution:
Unlock the lock screw located to the right of Terminal card.
Remove Control terminal card.
Then unlock the bottom cover.
Take a screw driver and pry open both sides of the bottom cover.
Remove the cover.



 

Was this helpful?
What can we do to improve the information ?