Technical FAQs

Ask a Question

Utilizing SoMove for an ATV61/71, can parameters and menus be made invisible to an operator using the keypad display?

Issue:
Is it possible to lock out menu headings via SoMove so that the customer can not see or access specific menus through the keypad on the ATV61/71 drive?

Product Line:
ATV61 / ATV71 drives with VW3A1101 graphic keypad

Environment:
All models, all serial numbers

Cause:
Customer wants to lock out certain menus to prevent unauthorized assess to the programming of the drive.

Resolution:
It is possible to block menu headings from view using SoMove.  The individual parameters under each menu heading can be blocked using the personalization tab within SoMove, but the menu headings will remain visible.

Use the keypad menu 7.3 PARAMETER ACCESS, Protection and Visibility settings to hide parameters and menus from view.
Was this helpful?
What can we do to improve the information ?