Technical FAQs

Ask a Question

Can the PowerSuite and SoMove configuration files be downloaded to the multiloader?

Issue:
Wants to copy a file from PowerSuite or SoMove directly to the Multiloader.

Product Line:
ATV61/71, ATV312, ATV12, ATV212, ATV32, ATS48, ATS22
Environment:
All models and serial numbers

Cause:
None

Resolution:
Yes, you can connect the Multiloader directly to a USB port on the PC.  It will look like a removable drive.  You can then save files to the Mutilloader as needed.

You can also remove the SD memory card from the Multiloader and plug that directly into an SD slot on the PC (if available) to do the same thing.

Consult the documentation that was provided with the Multiloader (document # BBV48787) for details.
Was this helpful?
What can we do to improve the information ?