Technical FAQs

Ask a Question

What is the part number for the heat sink fan on the ATV12 drive?

Issue:
ATV12 : What is the part number for the heat sink fan on the ATV12 drive?

Product Line:
Altivar . ATV12

Environment:
All models , all serial numbers

Cause:
Heatsink fan not running. 

Resolution:
There are no replacement parts available for the ATV12 . Replace the drive. 
Was this helpful?
What can we do to improve the information ?