Technical FAQs

Ask a Question

Is it possible to power the 230Vac ATV61 drive from DC Bus?

Issue:
Is it possible to power the  ATV61 drive 230Vac from DC Bus?

Product Line:
Altivar 61 ATV61

Environment:
230Vac , All series

Cause:
None

Resolution:
A separate DC source (approx 325Vdc) can be connected to PA/+ and PC/-  to power up the 230 Vac drive. DC Bus fuses are recommended for short circuit protection. No external Precharge resistor is necessary because it is built-in to the drive.
Was this helpful?
What can we do to improve the information ?