Technical FAQs

Ask a Question

Can an older monitor panel and CT`s from an old GC100 system be reused when retrofitting a newer GC200 relay?

No.  The old CT`s can still be used, but the monitor panel can not.  The GC 100 and GC200 relay systems are not compatible with each other.  Replace with all new monitor panels.

CTA-ID : 2050042
Was this helpful?
What can we do to improve the information ?