Technical FAQs

Ask a Question

What does voltage code M3X indicate in an ATV212HU40M3X drive part number ?

Issue: 
What does voltage code M3X indicate in an ATV212HU40M3X drive part number ?

Product Line: 
ATV212 Altivar212

Environment:
All

Cause: 
Order selection

Resolution: 
M3X indicates 200Vac / 240Vac -15% , +10% Three phase input.
Was this helpful?
What can we do to improve the information ?