Technical FAQs

Ask a Question

Are the ATV212 available in type 4 or 4X enclosure?

Issue:
Are the Altivar drives available in NEMA Type 4 or 4X enclosures?

Product Line
Altivar  

Environment
All

Cause:
Application request for Altivar NEMA type 4 or 4X enclosure

Resolution
There is not a standard offering for NEMA Type 4 or 4X enclosures for Altivar drives.
Was this helpful?
What can we do to improve the information ?