Technical FAQs

Ask a Question

Are the line and load voltage indicators field installable on safety switches?

Issue:
Application

Product Line:
Heavy Duty Safety Switch

Environment:
Applicaiton

Cause:
Customer would like to add voltage indicators after initial purchase.

Resolution:
These devices can ONLY be installed at the factory.  Please consult the latest Supplemental Digest for pricing.
Was this helpful?
What can we do to improve the information ?