Technical FAQs

Ask a Question

ATV32 can you reset a programmed function blocks via Ethernet?

Issue:
ATV32 can you reset the function blocks via Ethernet?

Product Line:
Alitvar ATV32

Environment:
All with Ethernet option card installed

Cause:
Needs to reset a function block via Ethernet.

Resolution:
Double click on that function bock input and assign it to C314. Then write it a decimal value of 16384
 

Was this helpful?
What can we do to improve the information ?