Technical FAQs

Ask a Question

Why does the multiloader not save the Safety functions (STO) in the ATV32?

Issue:
Why does the multiloader not save the Safety functions (STO) in the ATV32?

Product Line:
Altivar 32

Environment:
All models and serial numbers

Cause:
Product Design

Resolution:
It's an internal limitation. We want to have safety configuraiton only manageable with SoMove software. So the safety configuration is not saved in multiloader.

It's only possible to configure safety on ATV32 with SoMove one by one.
Was this helpful?
What can we do to improve the information ?