Technical FAQs

Ask a Question

Can Powerlink QOBPL breakers be ordered with longer leads?

Issue:
Can Powerlink QOBPL breakers be ordered with longer leads?

Product Line:
Powerlink PL

Environment:
All versions.

Cause:
Need to control panel further away

Resolution:
Powerlink QOBPL breakers can be order with extended leads by adding suffix (5392, 5393, 5394) to the base catalog number
5392 = 48 inch leads
5393 = 60 inch leads
5394 = 72 inch leads
Was this helpful?
What can we do to improve the information ?