Technical FAQs

Ask a Question

Is there a Feed-Thru Lug Kit available for the EZM11600TB or EZM31600TB Main Lug Terminal Box?

Application and Selection

Product Line:
EZM Tap Boxes

Need to feed lines through the tap box for multi-floor installation.

Yes, the EZM1600FTLK3 is the Feed-Thru Lug Kit for use with the EZM31600TB or EZM11600TB. This kit provides 24 additional lugs, 600 kcmil AL/CU, (6) per phase and neutral for a 3 phase/4 wire system. Six of the 24 additional lugs would not be used if the application is for a 1 phase/3 wire system.
Was this helpful?
What can we do to improve the information ?