Technical FAQs

Ask a Question

What is the part number for Simple Loader?

What is the part number for Simple Loader to use with the Altivar 12, 312, 32, 61 and 71 drives?

Product Line:
Altivar 12, 312, 32, 61, 71, ATV12, ATV312, ATV32, ATV61, ATV71

All catalog numbers

Need to copy and transfer the same program between multiple drives.

Part number for the Simple Loader is VW3A8120.

The Instruction Bulletin is document number 30072-452-46. 
Was this helpful?
What can we do to improve the information ?