Technical FAQs

Ask a Question

Where can the power dissipation value in Watts be found for the ATV71 drives?

Issue:
Power dissipation for the ATV71 drives.

Product Line:
ATV71 drives

Environment:
All

Cause:
Technical Support

Resolution:
This information can be found in the Global Catalog for the ATV71 catalog number 8800CT0501.

See section for Mounting and Installation recommendations.  The values in Watts are listed in the Power dissipated inside the enclosure table.
Was this helpful?
What can we do to improve the information ?