Technical FAQs

Ask a Question

Is there a way the ATV312 drive can detect an under current?

Issue:
Is there a way the ATV312 drive can detect an under current?

Product Line:
Altivar 312

Environment:
All models and serial numbers

Cause:
Need to configure the drive to indicate when an under current is attained to prevent damage to other equipment.

Resolution:
The Altivar 312 drive can use either the analog output or a relay output to indicate when a current threshold is attained.  A time delay must be used to disable the output when starting.
Was this helpful?
What can we do to improve the information ?