Technical FAQs

Ask a Question

Can an E-FLEX operate with single phase input?

Issue:
Can an E-FLEX operate with 230v single phase input?

Product Line:
Altivar 61, E-Flex

Environment:
All models, serial numbers and types

Cause:
None

Resolution:
The E-Flex was not designed for single phase input power.  Single phase power supply would violate the UL certification. Contact local PAE (Product Application Engineer) for assistance with this type of application.
 
Was this helpful?
What can we do to improve the information ?