Technical FAQs

Ask a Question

What is the generator interlock for the QO160M200PC Series S06 Load center?

Issue:
What is the generator interlock for the QO160M200PC Series S06 Load Center?

Product Line:
PTCCB - MCCBS,EARTH LEAK&SWITC

Environment:
60 Space Plug on Neutral Load Center

Cause:
Need for a generator interlock compatible with QO160M200PC.

Resolution:
Square D by Schneider Electric does not offer a generator interlock for the QO160M200PC Series S06 load center.

 
Was this helpful?
What can we do to improve the information ?