Technical FAQs

Ask a Question

Will the GS1QU3 disconnect switch accept more than one conductor on the line or load side?

Issue:
Will the GS1QU3 disconnect switch accept more than one conductor on the line or load side?
Product Line:
PTCTR-contactors
Environment:
GS1QU3
Cause:
Wiring termination
Resolution:
The lugs are double barrel design and accept 1-  #2 - 600KCMIL (CU/AL) in each barrel. So the lugs accept 2 conductors per phase.
Please see GIC Help files for this information.
 
Was this helpful?
What can we do to improve the information ?